|
This website is best viewed using Internet Explorer 6 and higher (IE 6.0) or Mozilla Firefox 1.5. The optimal resolution is 1024 x 768. Do not set your browser's Security Settings higher than medium.
To change resolution of your desktop, click on Start > Settings > Control Panel, choose the Display icon, then the Settings tab. Set the screen resolution slider to 1024 x 768.
To change the Security Settings of your IE browser, open a browser window. Click on Tools > Internet Options, then choose the Security tab. On the Security Level for this zone click the Default Level button, and set the slider to Medium or lower.
|