Cummins Northwest Specials
 
 
At Cummins Northwest, we understand the value of equipment up time and the need to accomplish timely and cost effective repairs when emergencies arise. Call any of our Cummins Northwest Service Centers to schedule a repair or click here to schedule service online for any of our service centers. And to help with your scheduled service event, ask our service representative how you can apply the 2010 Back on Track promotion certificate to your in shop service needs. Click here to download your 2010 Back on Track Certificate

M11 Overhaul
4025297 Overhaul Kit $3,172.36
4025298 OH Kit & 4952453RX Cylinder Head $4,565.35
The M11 Overhaul Kit includes: Pistons kits, Cylinder liner kits, Upper engine gasket set, Oil pan gasket set, Connecting rod bearings, Main bearing set, Tabbed crankshaft bearings

ISM Overhaul
4090008 OH Kit (Kit Only) $3,820.27
4090008 OH Kit & 4952453RX Cylinder Head (Kit & Head) $5,220.81
The ISM Overhaul Kit includes: Pistons kits, Cylinder liner kits, Upper engine gasket set, Oil pan gasket set, Connecting rod bearings, Main bearing set, Tabbed crankshaft bearings

'91 N14 Overhaul
4024877 / 78 OH Kit $1,852.09
OH Kit + 3 ReCon Heads $3,574.53
TriTech Plus Advantages vs. the Competition: An anodized combustion bowl, a longer piston pin with a contoured pin bore, and a Dual-Ni piston ring land insert for increased piston durability.
A 15-degree top ring keystone angle, an improved "I-shaped" oil ring, and advanced liner boring technology for improved oil control.
A 3 year/300,000 mile (482,700 km) warranty on the piston, rings, pin, liner, and liner o-ring seals.
The '91 N14 Overhaul Kit includes: TriTech Plus pistons w/ring packs and piston pins, LPF cylinder liner w/o-ring seals, Head gasket set, Oil pan gasket set, Connecting rod bearings, Main bearing set

'94 N14 Overhaul
4024879 / 80 / 81 OH Kit $3,736.70
4955558 / 59 / 60 (Oversized Liners) OH Kit $3,736.70
OH Kit + 3 ReCon Heads $4,965.22
Recon Cylinder Heads - Testing You Can Trust: Every Cummins ReCon N14 cylinder head is pressure tested twice to make sure there are no internal leaks in either the water jackets or the fuel lines. Every N14 casting is upgraded to the latest internal configuration as new heads, to improve injector sleeve durability. Sleeves are installed metal to metal, with no sealant to mask defects that could leak during operation. N14 heads feature 100% chrome exhaust valve stems and use an automated vacuum testing process to ensure the valves are properly seated to the valve seats. Critical parts, such as valve guides, sleeves, collets, and retainers are 100% replaced with only new genuine Cummins parts.
The '94 N14 Overhaul Kit includes: Connecting rod bearings, Articulated pistons w/ring packs and piston pins, LPF cylinder liners, Oil pan gasket set, Upper engine gasket set, Main bearing set

ISX Absolute Power
Cummins Northwest now offers ISX Overhaul kits in 3 versions: The Pre '02 ISX with Monothern conversion, the Pre '02 without Monothern conversion, and the '02 and later ISX EGR overhaul. The new Monothern piston design bundled with the overhaul kit is perfect to add power and performance back into the older ISX.
Improved power cylinder durability
Genuine Cummins Parts
Quieter cold start-ups
Superior oil control
Lower piston weight
Improved cylinder head gasket and hardened liners
Contact your Cummins Northwest service center for specific pricing for your ISX
Save up to $5,000 in truck idling fines!
Cover of Idle Talk Booklet
Today, state, provincial and local governments are creating idling legislation at an increasing rate. Some argue that federal-level rulings could bring order to this chaos. And this may yet happen. But the odds against relatively lax federal regulation overriding state and municipal law are not good. The trend, if anything, is toward stricter rules. In the meantime, the trucker is still at the mercy of local government enforcing a local noise ordinance applying to idling trucks. In New York, for example, truck drivers caught idling their engines for more than five minutes face fines up to $1,000
Did you know...
Truck drivers in New York who are caught idling their engines for more than five minutes face fines up to $1,000.
Truck drivers in Aspen, Colorado who are caught idling their engines for more than five minutes face fines up to $1,000 and/or one year of imprisonment.
In Toronto, Canada, idling more than three minutes could cost a truck driver up to $5,000 in fines.
"Idle Talk: How the Regulations Affect You" is a FREE 8-page guide created by Cummins Inc. It gives fleet owners and truck drivers a quick-reference of the latest maximum idling time allowed across the country, including a state-by-state overview and a list of Canadian regulations.